Skip to main content
PHolt.1
Senior
September 30, 2025
Question

32F417: How to use SWV ITM SWO debug output, without Cube IDE or even a debugger?

  • September 30, 2025
  • 22 replies
  • 1546 views

I have overall found this feature to be very unreliable, for reasons unknown. The data comes out OK from PB3 and goes all the way to the STLINK V3, at the expected speed, 1MHz, but Cube IDE displays nothing. I have this across a number of development units. Sometimes it works and then stops...

Anyway, digging into this, it looks like the entire trace macrocell is configured via the debugger when (or before) reset is released from the target. That is why none of the STM example code sets up any of this stuff. I also managed, years ago, to get SWV working not with Cube IDE but with the STM32 STLINK Utility, which presumably does the same via-debugger config tricks.

Also just because you see 1MHz stuff on the scope doesn't mean that it is in the right format for Cube IDE to decode it.

So I went looking for how to get this stuff configured in software in the target. Obviously any such config will override the Cube/debugger config so you will have to make sure Cube IDE's config matches exactly if you still want that to work. And after a lot of work I found the following, and wonder whether it is complete:

1) Set up PB3 to be an output, probably fast mode, and enable portb clock.

2) Set up the macrocell. I found this on this ST forum

/*
	Initialize the SWO trace port for debug message printing
	portMask : Stimulus bit mask to be configured
	cpuCoreFreqHz : CPU core clock frequency in Hz
	baudrate : SWO frequency in Hz
*/
 
void swoInit (uint32_t portMask, uint32_t cpuCoreFreqHz, uint32_t baudrate)
{
	uint32_t SWOPrescaler = (cpuCoreFreqHz / baudrate) - 1u ; // baudrate in Hz, note that cpuCoreFreqHz is expected to match the CPU core clock
 
	CoreDebug->DEMCR = CoreDebug_DEMCR_TRCENA_Msk; 		// Debug Exception and Monitor Control Register (DEMCR): enable trace in core debug
	DBGMCU->CR	= 0x00000027u ;							// DBGMCU_CR : TRACE_IOEN DBG_STANDBY DBG_STOP 	DBG_SLEEP
	TPI->SPPR	= 0x00000002u ;							// Selected PIN Protocol Register: Select which protocol to use for trace output (2: SWO)
	TPI->ACPR	= SWOPrescaler ;						// Async Clock Prescaler Register: Scale the baud rate of the asynchronous output
	ITM->LAR	= 0xC5ACCE55u ;							// ITM Lock Access Register: C5ACCE55 enables more write access to Control Register 0xE00 :: 0xFFC
	ITM->TCR	= 0x0001000Du ;							// ITM Trace Control Register
	ITM->TPR	= ITM_TPR_PRIVMASK_Msk ;				// ITM Trace Privilege Register: All stimulus ports
	ITM->TER	= portMask ;							// ITM Trace Enable Register: Enabled tracing on stimulus ports. One bit per stimulus port.
	DWT->CTRL	= 0x400003FEu ;							// Data Watchpoint and Trace Register
	TPI->FFCR	= 0x00000100u ;							// Formatter and Flush Control Register
 
	// ITM/SWO works only if enabled from debugger.
	// If ITM stimulus 0 is not free, don't try to send data to SWO
	if (ITM->PORT [0].u8 == 1)
	{
		bItmAvailable = 1 ;
	}
}

 What I don't get however is the comment "ITM/SWO works only if enabled from debugger.". What is this about? There may not be a debugger!

The actual output function is the usual ST one:

// Copy of the one in core_cm4.h
static inline void ITM_SendChar (uint32_t ch)
{
 if (((ITM->TCR & ITM_TCR_ITMENA_Msk) != 0UL) && /* ITM enabled */
 ((ITM->TER & 1UL ) != 0UL) ) /* ITM Port #0 enabled */
 {
 while (ITM->PORT[0U].u32 == 0UL)
 {
 __NOP();
 }
 ITM->PORT[0U].u8 = (uint8_t)ch;
 }
 return;
}

 

22 replies

Andrew Neil
Super User
September 30, 2025

@PHolt.1 wrote:

I found this on this ST forum


Please give a link to where you found it.

 


@PHolt.1 wrote:

What I don't get however is the comment "ITM/SWO works only if enabled from debugger.". What is this about?

Some debug features are only accessible via a debugger - the CPU has no access.

See also DHCSR in Cortex-M0.

PS:

ARM document accessible registers here.

ARM's SWO documentation here.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PHolt.1
PHolt.1Author
Senior
September 30, 2025

It is in this thread

https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-enable-swo-with-st-link-utility-on-stm32f407g-disc1/td-p/228896

Re with-debugger-only operation, I recall reading that the SWO output can be used without a debugger. It seems to be just a UART. The above link and the code there suggests that is the case, otherwise who would bother?

You can also look here

https://gist.github.com/mofosyne/178ad947fdff0f357eb0e03a42bcef5c

which contains similar stuff.

Andrew Neil
Super User
September 30, 2025

@PHolt.1 wrote:

It seems to be just a UART.

AIUI, one of the supported SWO protocols is UART:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/uart-signal-on-swo-pin-from-st-link-v2-3/m-p/742817/highlight/true#M22588

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PHolt.1
PHolt.1Author
Senior
September 30, 2025

Yes; it supports various encodings including Manchester, but AFAICT the 32F4 to STLINK V3 to Cube IDE interface is just a standard NRZ UART.

Presumably one doesn't have (up to) 12MHz NRZ going back to the PC via USB :) so the reception must be implemented by the STM CPU in the debugger (32F723 in the little one I am looking at) which packages the data and buffers it for the PC host to retrieve it over USB.

Looking at it on a scope, it looks like a standard microcontroller UART i.e. normally high, with a start bit going low. But I can't be sure.

It would be interesting if it could be used as a standalone output. I cannot find details of these registers anywhere e.g.

TPI->FFCR	= 0x00000100u ;	

 

EDIT:

This

https://www.eevblog.com/forum/microcontrollers/stlink-debugger-configures-some-32f4-target-registers-e-g-swo-trace-macrocell/msg6054147/#msg6054147

shows that what I want is basically impossible.

So back to why SWV ITM is not working :)

AScha.3
Super User
September 30, 2025

>So back to why SWV ITM is not working :)

It IS working...if you do it right, not sooo difficult (but not always working instantly...dont ask me why.).

1. its not working without debug/st-link , because the debug unit has to know, it should do it now.

2. you could write these instructions yourself, without "debug" active, as shown in your link (gist/git...).

3. to send on printf(...) you only need:  (at end of main, see user code marks)

/* USER CODE BEGIN 4 */

int __io_putchar(int ch)
{
 ITM_SendChar(ch);
 return (ch);
}

/* USER CODE END 4 */

...then send is simple as:

 printf("**** start *******\r\n"); // always \n needed !

+

enable in debug SWV: (cpu core clock has to be the real clock value ! !  here 200MHz )

AScha3_1-1759250842708.png

+

set itm0 , when debug started, wait at main, in SWV settings:

AScha3_0-1759250674533.png

+ "start" with the red button

-> then run program and get the messages you send:

AScha3_2-1759250958359.png

btw

sometimes its not working on the first run, end debug, start it again, red button again...

funny: if its working, its always working, also after mod code, compile, debug...no need to start it again... :)

+

Without debug etc its more easy and straight : use one of the many uarts, set it on (i do) 3 Mbit, transmit only;

on a plug you can connect to a running machine and see the messages, without stopping or changing the "normal" running status; no debug session needed.

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
September 30, 2025

You have to disable PC Sampling.

I posted it here

https://www.eevblog.com/forum/microcontrollers/stlink-debugger-configures-some-32f4-target-registers-e-g-swo-trace-macrocell/msg6054397/#msg6054397

PC Sampling is only for the SWV Statistical Profiling feature. I don't think you can have SWV ITM debugs and Statistical Profiling running concurrently.

In fact I now find Statistical Profiling is very hard to get working, but I used it successfully a few years ago (earlier version of Cube than my 1.14.1).

BTW I froze Cube at 1.14.1 because later versions don't fix anything, and mostly broke the debugger.

 

 

Pavel A.
October 1, 2025

> What I don't get however is the comment "ITM/SWO works only if enabled from debugger.". What is this about? There may not be a debugger!

The meaning of "debugger" here is the any external software or firmware that drives the SWD interface from outside.

 

AScha.3
Super User
October 1, 2025

@Pavel A. 

Not driving, it just has to be programmed to do the SWV output, as the debug unit is sleeping or waiting to do something at startup, but you want it to do something.

So you use the debug st-link to set it to the desired mode.

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
October 1, 2025

It seems clear from the EEVBLOG thread (link above) that the SWO cannot be used as a simple UART. The data is encoded in some complicated way. In fact, on a scope I see continuous data, with what looks like a 2 byte packet coming out every 90us. And continuous data going into the target from the debugger.

That code above for enabling SWO is a redherring. It is for the narrow application scenario of some 3rd party OpenOCD debugger, and then the target needs to run some code to set it up. With Cube IDE + STLINK, the debugger uses the SWD interface to set up the target CPU trace macrocell entirely.

The general reliability issues remain, however, and AFAICT disabling PC Sampling is now a requirement for the SWV ITM debug console to work. I can reproduce this across several targets and operating systems.

AScha.3
Super User
October 1, 2025

>disabling PC Sampling is now a requirement for the SWV ITM debug console to work.

No, just think: there is a buffer with fixed size (2MB or so) and if you switch on sampling, it is filled quite fast, depending on sampling rate. So if you want see the cpu/task statistics , you only can run the from debug/pause to pause debug again some seconds or minutes (set buffer to 10x default size, as i do, helps for longer statistics);

then switch off sampling , or if want statistics again, clear the trace buffer. (Same with live watching -> graph.)

To adapt to the resolution of sampling you need, set the prescaler (longer time for sampling, but lower time resolution.)

So usually sampling has to be off, to run only SWV messages and view them in swv console without filling the buffer in short time.  And set more buffer size  than default,  for more/longer sampling time.

 

AScha3_0-1759304677029.png

 

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
October 1, 2025

I already have a huge buffer set there.

I have some SWV debugs at the very start of my program, active a fraction of a second after start, and absolutely nothing, zero, zilch, nowt, comes out, if the PC Sampling option is enabled.

It may well be a SWD bandwidth issue but I have played with the clock speeds and see no change. Even the non isolated very latest STLINK V3 MINIE shows the same behaviour, and I would expect that one to be super fast.

Very probably I never had PC Sampling enabled when I used SWV ITM extensively in the past. I would have enabled it for the performance profiling feature and just forgot to turn it off.

This is Cube IDE 1.14.1. Later versions usually broke the debugger until a fix in version x.x.1 so I stopped bothering :)

Can you or anyone check if SWV ITM works with PC Sampling enabled and, if yes, post screenshots of config?

If nobody responds then it probably never worked.

AScha.3
Super User
October 1, 2025

Yes, as i said: working fine, see here example for profiling: maybe one minute running (top part...> 1%)

AScha3_1-1759315476613.png

+

>This is Cube IDE 1.14.1. Later versions usually broke the debugger 

Yes, i also didnt update...until "forced to do" , because for new cpu you need new IDE/Cube .

But just the last versions 1.18.1 and 1.19.0 now - maybe the "best ever" , everything working as it should. A wonder. :)

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
October 1, 2025

What I meant was: with PC Sampling enabled, does the SWV ITM debug console work for you?


How do you set the address range for profiling?

I cannot get it to show more than a bit of the startup code, in the bottom 32k block.

The buffer is set to 20MB.

AScha.3
Super User
October 1, 2025

>with PC Sampling enabled, does the SWV ITM debug console work for you

Yes, ok, until buffer full....then error message.

As i said: not for running long time with profiling.

+ set prescaler :because SWV is in the end a serial, at 2 or ...8 mbit , so it cannot send sampling time info at a rate of 100 MHz or so...i have prescaler set to 64 or more...at 200MHz core speed.

Buffer i have also at 20MB for profiling.

+

>How do you set the address range for profiling?

Huh, what?   Profiling just gives you the time/function in % , = how long is cpu busy in ...,...,...;

no address range, just all, what its doing, while sampling.

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
October 1, 2025

What settings do you have here?

PHolt1_0-1759324842712.pngPHolt1_1-1759324875407.png

 

AScha.3
Super User
October 1, 2025

...about same (just other cpu , H743 H7A3 , clock etc. );

and debug (mostly i use OCD ) software reset:

AScha3_0-1759325622977.png

+

uncheck PC sampling, if not looking for statistics.

 

If you feel a post has answered your question, please click on " Best Answer ".
PHolt.1
PHolt.1Author
Senior
October 1, 2025

OCD... what debugger?

Yes I have to uncheck PC Sampling for SWV ITM to work.

I have tried OCD with the CTLINK V3 and it does exactly the same stuff as with SWD.