Skip to main content
Associate II
August 11, 2023
Solved

STM32H563VI Octo-SPI interface dummy cycles

  • August 11, 2023
  • 4 replies
  • 4403 views

Hi,

someone can explain me how to calculate the "dummy cycles" number reading an external flash qspi such as the Winbond W25Q64JV ?

I have to read in qspi mode with the Fast Read Quad I/O (EBh) command in SDR mode. The flash memory datasheet asks for 4 dummy cycles between addressing and data available.

In effect, if I set 4 dummy cycles, the first data byte is lost. On the contrary, if I set 6 dummy cycles, the read operation success.

I think this depend to the Pre-drive time, but how can I calculate the effective dummy cycles to apply, to be sure that all the reading will be done correctly ?

Thank you.

This topic has been closed for replies.
Best answer by Tesla DeLorean

It's 6 in your case because you fail to deal with the Mode/Alternate bits that the part is expecting...

w25q64_eb_cmd.jpg

4 replies

Foued_KH
ST Employee
August 11, 2023

Hello @Ez_it , 

I think that you can contact the manufacture for more details because the datasheet refer to 4 dummy cycles 
"four Dummy clocks are required in SPI mode prior to the data output"

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ez_itAuthor
Associate II
August 11, 2023

Hi Foued,

thank you for your answer but in the STM32H5xx reference manual there is this figure about the dummy cycles

Ez_1-1691760700806.png

As you can see, the Dummy Cycles contains a "Pre-Drive" time that is not described in anywhere, and moreover in the same Reference Manual, speaking about the Dummy Cycle Phase, I found this:

Ez_2-1691760868906.png

What does it mean "there must be at least one dummy cycle" ....?? Means one, two, three, or so many?

In my opinion, I have to clarify this before ask to the memory manufacturer, because it is not clear.

Moreover, I found some drivers for the same flash memory on GitHub where the dummy cycles has been increased to 6, I think for the same reason:

https://github.com/Crazy-Geeks/STM32-W25Q-QSPI/blob/main/Library/w25q_mem.c

where you can find:

/**
* @brief W25Q Read any 8-bit data from raw addr
* Read any 8-bit data from preffered chip address
*
* @note Address is in [byte] size
* @note Be carefull with page overrun
* @PAram[out] buf Pointer to data to be written (single or array)
* @PAram[in] data_len Length of data (1..256)
* @PAram[in] rawAddr Start address of chip's cell
* @return W25Q_STATE enum
*/
W25Q_STATE W25Q_ReadRaw(u8_t *buf, u16_t data_len, u32_t rawAddr) {
if (data_len > 256 || data_len == 0)
return W25Q_PARAM_ERR;

while (W25Q_IsBusy() == W25Q_BUSY)
w25q_delay(1);

QSPI_CommandTypeDef com;

com.InstructionMode = QSPI_INSTRUCTION_1_LINE; // QSPI_INSTRUCTION_...
#if MEM_FLASH_SIZE > 128U
com.Instruction = W25Q_FAST_READ_QUAD_IO_4B; // Command
com.AddressSize = QSPI_ADDRESS_32_BITS;
#else
com.Instruction = W25Q_FAST_READ_QUAD_IO; // Command
com.AddressSize = QSPI_ADDRESS_24_BITS;
#endif
com.AddressMode = QSPI_ADDRESS_4_LINES;

com.Address = rawAddr;

com.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
com.AlternateBytes = QSPI_ALTERNATE_BYTES_NONE;
com.AlternateBytesSize = QSPI_ALTERNATE_BYTES_NONE;

com.DummyCycles = 6;
com.DataMode = QSPI_DATA_4_LINES;
com.NbData = data_len;

com.DdrMode = QSPI_DDR_MODE_DISABLE;
com.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
com.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

if (HAL_QSPI_Command(&hqspi, &com, HAL_QSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK)
return W25Q_SPI_ERR;

if (HAL_QSPI_Receive(&hqspi, buf, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
return W25Q_SPI_ERR;

return W25Q_OK;
}

 

 

 

 

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
August 11, 2023

It's 6 in your case because you fail to deal with the Mode/Alternate bits that the part is expecting...

w25q64_eb_cmd.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ez_itAuthor
Associate II
August 11, 2023

you are a genius :grinning_face: