Associate
August 3, 2023
Solved
STM32G070 ADC DMA - Invalid value in array.
- August 3, 2023
- 4 replies
- 3250 views
Hi.
I am using STM32G070RB.
I need to sequentially receive values from 5 channels using ADC DMA.
If normal circumstances, the ADC data of PA0 should be stored in Array[0] and the ADC data of PA1 should be stored in Array[1].
However, currently experiencing a bug where PB0's ADC data is stored in Array[0], and PA0's ADC data is stored in Array[1].
PB0's ADC data is a variable value, and the ADC data of other pins is a fixed value.
PB0's ADC data should come out with continuously changing values in the array[4].
Can you give me some advice where i made a mistake?





main.c
void ADC_DMA_TC_Callback()
{
asm("nop");
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_USART3_UART_Init();
MX_TIM15_Init();
MX_TIM16_Init();
/* USER CODE BEGIN 2 */
LL_ADC_StartCalibration(ADC1);
while(LL_ADC_IsCalibrationOnGoing(ADC1));
LL_DMAMUX_SetRequestID(DMAMUX1, LL_DMAMUX_CHANNEL_0, LL_DMAMUX_REQ_ADC1);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_1, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_1, LL_ADC_DMA_GetRegAddr(ADC1, LL_ADC_DMA_REG_REGULAR_DATA));
LL_DMA_SetMemoryAddress(DMA1, LL_DMA_CHANNEL_1, (uint32_t)ADCVal);
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_1, 5);
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_1);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_1);
LL_ADC_Enable(ADC1);
while (LL_ADC_IsActiveFlag_ADRDY(ADC1) == 0);
//LL_TIM_EnableCounter(TIM15);
LL_ADC_REG_StartConversion(ADC1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}stm32g0xx_it.c
void DMA1_Channel1_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Channel1_IRQn 0 */
if(LL_DMA_IsActiveFlag_TC1(DMA1))
{
LL_DMA_ClearFlag_TC1(DMA1);
ADC_DMA_TC_Callback();
}
/* USER CODE END DMA1_Channel1_IRQn 0 */
/* USER CODE BEGIN DMA1_Channel1_IRQn 1 */
/* USER CODE END DMA1_Channel1_IRQn 1 */
}