Skip to main content
Senior
July 11, 2023
Solved

ADC and pullup/pulldown

  • July 11, 2023
  • 8 replies
  • 14909 views

Hi, for a STM32F303RE I configured a pin as an ADC input. I want to use the pullup/pulldown resistors as a voltage divider for an offset voltage. I tried to switch on both in ADC mode, that did not work. Everything is fine with the pin configured as an input. 

Is there a solution to this?

THX 

Cheers 

Detlef 

This topic has been closed for replies.
Best answer by Nikita91

Yes you can configure the GPIO as input with pull-up, then use the ADC on this pin. (The analog path go straight from the pin to the ADC input). But the schmitt trigger is activated so the ADC quality is altered (digital noise injected). 

This was already discussed here: https://community.st.com/t5/stm32-mcu-products/adc-and-gpio-input-modes/td-p/529797 

8 replies

Nikita91
Lead II
July 11, 2023

GPIO pull up/down is not allowed in analog mode.

Have look in the reference manual "11.3 GPIO functional description". Pull up/down is only mentioned for input and output mode.

It is not a good idea to use the internal pull up for a voltage divisor as the resistor value margin is large: 25 to 55 KOhms.

The solution: use an external divisor...

 

DetlefSAuthor
Senior
July 11, 2023

Hi Nikita, so I can toggel the mosfet switches for pull up/down resistors only in input/output mode of the pin? Not in ADC mode? No workarounds, no hidden and secret bits? I do not care about any volatile DC offset. 2 saved Rs for hundred million devices makes a nice beach villa. 

Thx

Cheers

Detlef 

Michal Dudka
Lead
July 11, 2023

In "Analog" mode you are not able to activate internal pullup or pulldown.
In "input" mode you can activate pulldown or pullup, but not both of them at the same time and you are still able use pin as source for ADC. But you have to count with some small injection currents (up to 100nA ?). These will most likely be negligible compared to the variance of pullup/pulldown resistance... you can save one resistor.

DetlefSAuthor
Senior
July 11, 2023

Hi, in input mode I can use the same pin as ADC, no? How that? Sure you can switch on both pull up/down in input mode. You have two bits for that, fourth case is marked as " reserved" but it switches on both resistors.

Michal Dudka
Lead
July 12, 2023

I've tested this "reserved" combination (0b11) at STM32F042 with negative result (both resistors were disabled in that state)... did you succefuly tested that ? 

Nikita91
Nikita91Best answer
Lead II
July 12, 2023

Yes you can configure the GPIO as input with pull-up, then use the ADC on this pin. (The analog path go straight from the pin to the ADC input). But the schmitt trigger is activated so the ADC quality is altered (digital noise injected). 

This was already discussed here: https://community.st.com/t5/stm32-mcu-products/adc-and-gpio-input-modes/td-p/529797 

DetlefSAuthor
Senior
July 12, 2023

Hi Nikita, I got it.

THX

Cheers

Detlef