Skip to main content
EKore.1
Associate II
July 27, 2020
Solved

What are the differences between ST25DV04K and M24SR64-Y? Is ANT7-T-ST25DV04K compiles to FCC like ANT7-T- M24SR64-Y?

  • July 27, 2020
  • 2 replies
  • 1096 views

..

This topic has been closed for replies.
Best answer by Peter BENSCH

ST25DV: based on ISO/IEC 15693

M24SR: based on ISO/IEC 14443 A

Additionally: ST25DV04K provides 4kbit, while M24SR64 provides 64kbit (even that is very obvious... :smiling_face_with_smiling_eyes:)

FCC:  ANT7-T-ST25DV04K is not listed at FCC, while the X-NUCLEO-NFC04A1 is.

Does it help?

Good luck!

/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 31, 2020

ST25DV: based on ISO/IEC 15693

M24SR: based on ISO/IEC 14443 A

Additionally: ST25DV04K provides 4kbit, while M24SR64 provides 64kbit (even that is very obvious... :smiling_face_with_smiling_eyes:)

FCC:  ANT7-T-ST25DV04K is not listed at FCC, while the X-NUCLEO-NFC04A1 is.

Does it help?

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
EKore.1
EKore.1Author
Associate II
August 2, 2020

Thanks