Skip to main content
dipti23
Visitor II
February 16, 2015
Solved

Tag ANT-M24LRA not getting detected by Lumia 830

  • February 16, 2015
  • 1 reply
  • 565 views
Posted on February 16, 2015 at 07:45

Microsoft in Windows phone 8.1 has added new Nfc related features including low level access(Non NDEF). I have Nokia Lumia 830 (PN547 NFC chipset is present in this device).Im not able to detect Nfc tag (ANT-7M24LR-A ,ISO15693) through Lumia 830, which im able to read/write using Nfc-V(ISO15693) in Android. I also have a Lumia 720 (old NFC hardware) but atleast it is able to detect the tag. Has anyone encountered this ? Whats the workaround ?

#m24lr #lumia
This topic has been closed for replies.
Best answer by Anais GALLIGANI
Posted on June 26, 2015 at 16:19

Good day Gokhale,

This is unforunately normal, on this lumia the ISO 15693 is not allowed.

(on the new generation of Microsoft phone, ISO 15693 will be supported)

You can try to use M24SR-DISCO-PREM, that can be use with Lumia NFC enabled phone.

I hope this is helping,

I wish you a great day,

ST NFC/RFID Dynamic support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
June 26, 2015
Posted on June 26, 2015 at 16:19

Good day Gokhale,

This is unforunately normal, on this lumia the ISO 15693 is not allowed.

(on the new generation of Microsoft phone, ISO 15693 will be supported)

You can try to use M24SR-DISCO-PREM, that can be use with Lumia NFC enabled phone.

I hope this is helping,

I wish you a great day,

ST NFC/RFID Dynamic support