cancel
Showing results for 
Search instead for 
Did you mean: 

I use st25r3916 , How do I read and write 14443a tag block? Is there a ready-made function interface

xxiao.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

Do you use a X-NUCLEO-NFC06A1 board (and X-CUBE-NFC6 Firmware) or a ST25R3916-DISCO board (and STSW-ST25R010 PC software) or a custom board (and ST RFAL firmware)?

ISO14443-3 does not define any tag memory organization. Different kinds of tags are relying on ISO14443-3 :

  • T1 tags
  • T2 tags
  • T4 tags
  • proprietary tags

If you are using the ST RFAL,

  • see rfal_t1.c for T1 tag read/write API
  • see rfal_t2.c for T2 tag read/write API
  • see rfal_t4.c for T4 tag helpers API

Feel free to share more details about your tag (manufacturer an model).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

Do you use a X-NUCLEO-NFC06A1 board (and X-CUBE-NFC6 Firmware) or a ST25R3916-DISCO board (and STSW-ST25R010 PC software) or a custom board (and ST RFAL firmware)?

ISO14443-3 does not define any tag memory organization. Different kinds of tags are relying on ISO14443-3 :

  • T1 tags
  • T2 tags
  • T4 tags
  • proprietary tags

If you are using the ST RFAL,

  • see rfal_t1.c for T1 tag read/write API
  • see rfal_t2.c for T2 tag read/write API
  • see rfal_t4.c for T4 tag helpers API

Feel free to share more details about your tag (manufacturer an model).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.