Skip to main content
mdiet.1
Associate
April 29, 2022
Solved

How do i get into testmode with continuous unmodulated / modulated field

Hello,

For various tests and especially for certification, I like to put the ST25R39xx into a test state in which it generates a continuous unmodulated field or a field modulated with random data (similar to NXP's PRBS test).

Is such a mode available?

How can I access this mode? Ideally via the RFAL library.

The ST25R3916-DISCO board is FCC certified. Can you share the project / code used for FCC certification?

Thanks in advane,

Michael

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
May 6, 2022

Hi Michael,

please use rfalSetMode() instead/before rfalSetBitRate() to explicitly define the to be used technology.

Of course also the rfalWorker() needs to be called until rfalGetTransceiveStatus() does not return ERR_BUSY anymore.

The GT is for delaying the first command after the field on by typically 5ms. There is no automatic field off (except if you use AP2P). Then afterwards the software makes sure to employ an FWT of 500us between the frames being sent.

Best Regards, Ulysses

3 replies

Ulysses HERNIOSUS
ST Technical Moderator
April 29, 2022

Hi Michael,

don't have the details of testing at hand but the tests were either performed at constant carrier (rfalFieldOnAndStartGT()) or during running polling loop.

If you would want to have frames with PRBS pattern you would need to select it and send the frames using one of the supported technologies (rfalStartTransceive(), etc.).

Best Regards, Ulysses

mdiet.1
mdiet.1Author
Associate
May 6, 2022

Hello Ulysses,

​

thank you for your help.

​

So can I only use the functions from rfal_rf.h for this and after an initialization consisting of

​

rfalInitialize(),

rfalSetBitRate(),

rfalFieldOnAndStartGT()

​

and then execute

​

rfalStartTransceive(),

rfalGetTransceiveStatus()

​

in a loop?

​

Does the GT (Guard Timer?) turn the field off after an timeout?

​

I need no communication with an transpondercard, only an permanent and modulated carrier with the specified bitrate.

​

Thanks,

Michael

​

Ulysses HERNIOSUS
ST Technical Moderator
May 6, 2022

Hi Michael,

please use rfalSetMode() instead/before rfalSetBitRate() to explicitly define the to be used technology.

Of course also the rfalWorker() needs to be called until rfalGetTransceiveStatus() does not return ERR_BUSY anymore.

The GT is for delaying the first command after the field on by typically 5ms. There is no automatic field off (except if you use AP2P). Then afterwards the software makes sure to employ an FWT of 500us between the frames being sent.

Best Regards, Ulysses