cancel
Showing results for 
Search instead for 
Did you mean: 

STWBC2-HP and STWLC99: output only reaches 0.8A - expecting 5A

Fengji
Associate II

I am using STWBC2-HP and STWLC99 for development. The output voltage at the receiver end is set to 10V, and the current limit at the transmitter end is set to 5A. However, the actual current at the transmitter end can only reach a maximum of 0.8A, and I do not know why.

13 REPLIES 13
Didier HERROUIN
ST Employee

Hello,

ST has decided to limit its offer in terms of power (30W) and in terms of portfolio.

We focus now on 4 products : the STWBC86 (up to 5W) + the STWBC2-HP (up to >30W) for Transmitter side and the STWLC38 (up to 15W) + the STWLC89 (up to 20W, Qi 2.0 MPP) for Rx.

Unfortunately, the STWLC99 has been stopped.

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Although your STWLC99 has been discontinued, I have already purchased ST's products, and I should receive the support I am entitled to. The issue I am facing now is that the output current of the STWBC20-HP can only reach 0.8A. I need to resolve the problem on the transmitter side, not the STWLC99.
 
Didier HERROUIN
ST Employee

Hello,

Yes of course.

Please open a case on st.com (https://www.st.com/content/st_com/en/support/support-home.html#), you ticket should be re-directed to me and I will be able to support you directly.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I purchased the development boards and chips from your distributor. If you need it, I can provide you with the order.

No, I do not have access to the distributors orders list.

You may ask your distributor to open a case for you, and your distributor may add your email address in the case so that I can contact you directly.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

My agent wants to know how to operate, as they have not opened a case before.

The generic OLS portal can be found at this address : ols home

Please fill it carefully with the right product name (STWBC2-HP) and in the comment, you can add : Please assign this ticket to Didier Herrouin.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

My supplier has already submitted the case, but I haven't received any email from anyone.

Didier HERROUIN
ST Employee

Do you have the number of the case ?


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.