cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ISV020V1 increase VEOC

rsmqu
Associate II

Hi @Peter BENSCH can you help me how to modify the  STEVAL-ISV020V1 to make the VEOC up to 5.3V?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Well, the data sheet, section 6.1 describes how VEOC is set with a voltage divider R4, R5, R6. The same designations of the resistors can also be found in AN4397, where the equations 12...14 in section 4.3.3 only have to be rearranged according to the required resistance (VBG = Bandgap Reference Voltage = typ 1.23V).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Well, the data sheet, section 6.1 describes how VEOC is set with a voltage divider R4, R5, R6. The same designations of the resistors can also be found in AN4397, where the equations 12...14 in section 4.3.3 only have to be rearranged according to the required resistance (VBG = Bandgap Reference Voltage = typ 1.23V).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Can you share me a schematic diagram to make the VEOC up to 5.3V?

Peter BENSCH
ST Employee

The schematic for this is identical to a smaller VEOC, only the resistors R4, R5 and R6 have to be adapted. Please read the sections mentioned in the data sheet and AN4397 and try to transform the equations.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.