2021-11-22 10:17 PM
Hello,
I am working with STC3115 and I would like to know, the maximum charging current that I can measure with it?
Solved! Go to Solution.
2021-11-23 5:16 PM
Given the calculation:
Vin_gg = Rcg * IMaxwith maximum input voltage (Vin_gg) at 40 mV and minimum current sense resistor (Rcg) at 5 mohm,
the maximum application charging current (IMax) will be 8A.
2021-11-23 2:48 AM
Well, that is a question of design: the battery current is not measured directly, but via a shunt, which is why there is theoretically no upper limit.
However, the internal Sigma-Delta ADC is limited to 14bit and has a typical LSB value of 5.88µV. So the larger you make the current, the lower the resistance of the shunt and the coarser the measurement will be.
Regards
/Peter
2021-11-23 5:16 PM
Given the calculation:
Vin_gg = Rcg * IMaxwith maximum input voltage (Vin_gg) at 40 mV and minimum current sense resistor (Rcg) at 5 mohm,
the maximum application charging current (IMax) will be 8A.
2021-11-23 8:27 PM
Thanks, Peter for your prompt reply.
2021-11-23 8:28 PM
Thanks, Winfred for your prompt explanation.