cancel
Showing results for 
Search instead for 
Did you mean: 

Start up L6981(C33) problems

Chris_SA
Associate II

I'm using the L6981C33DR bug converter to convert 24V (from an SDR-120-24 power supply) down to 3.3V. However, I've had instances where the regulator overheats and "exploaded".

The circuit only needs to supply around 100mA at startup, so the current draw isn't excessive. My suspicion is that there might be a voltage spike at startup that occasionally damages the regulator, but it happens infrequently and I haven't been able to capture it on an oscilloscope.

Has anyone encountered a similar issue or have any insights on how to troubleshoot this?

I've attached a picture of the schematic and PCB layout for reference. Any guidance or suggestions are greatly appreciated, and I'm happy to provide additional information if needed.

Chris_SA_0-1731060300492.png

Chris_SA_1-1731060609394.png

 

Chris Salimans

1 ACCEPTED SOLUTION

Accepted Solutions
Chris_SA
Associate II

I found the problem. the 24V was via a connector, when plugging this connector in it made a smal spark what probably made the voltage for a realy short time below or above the max voltage of the chip. Solved it with a 1uh condensator and a TVS over 24V and gnd.

View solution in original post

7 REPLIES 7
AScha.3
Super User

>supply around 100mA at startup

And then..? avg. out current ?

 

 

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for following up! The total maximum current is around 500mA, but when the issue happens, it’s far below that, just powering some LEDs and a microcontroller.

Peter BENSCH
ST Employee

@Chris_SA What type of inductor do you use?

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

OK, I was afraid that you were using a magnetically unshielded coil and would inductively feed switching pulses from the coil back into the FB pin, which could lead to oscillation and thus great instability. But the 744777133 is actually magnetically shielded.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Chris_SA
Associate II

It might have something to do with the inductor value.

I selected the predefined value for 3.3V, but it could be too high or too low for my application?

Chris_SA
Associate II

I found the problem. the 24V was via a connector, when plugging this connector in it made a smal spark what probably made the voltage for a realy short time below or above the max voltage of the chip. Solved it with a 1uh condensator and a TVS over 24V and gnd.