Is FOD supported both in TX and RX ICs or only one side of the power transfer components taking care of this?
Is FOD (Foreign Object Detection) supported both in TX and RX ICs or only one side of the power transfer components taking care of this?
FOD tuning is required for both Rx and TX. The TX assumes the role to trigger FOD. Both of our Tx devices support FOD and the tuning. Based on the application, ST Rx devices need to be fine-tuned in terms of adjustment of the accuracy of the Received Power Packet which is sent periodically to the Tx and used by Tx for FOD evaluation.