2021-01-26 3:48 AM
2021-02-04 6:56 AM
Hello @GMoha.1,
the STEVAL-PTOOL2V1 is a reference design for power tools.
The driving method of this kind of application is the 6-step with position feedback from phase Hall-effect sensors.
The board is configured with a single shunt sensing topology and a companion STSW-PTOOL2V1 firmware is provided for evaluation.
Let me know if I solved your doubts, if so please "Select as Best" button.
2021-02-04 6:56 AM
Hello @GMoha.1,
the STEVAL-PTOOL2V1 is a reference design for power tools.
The driving method of this kind of application is the 6-step with position feedback from phase Hall-effect sensors.
The board is configured with a single shunt sensing topology and a companion STSW-PTOOL2V1 firmware is provided for evaluation.
Let me know if I solved your doubts, if so please "Select as Best" button.
2021-02-18 4:25 AM
Hello @GMoha.1 any feedback from you?
We can consider closed this topic?
2021-08-05 7:44 AM
Hi,
Your answer did not help us. I was trying to do the same think. Adding support of the STEAVL-PTOOL2V1 to Motor control Workbench would be great. I try to generate a Cube IDE project with Motor Control Workbench, but without the board in the list it wasn't easy for first user.
Other solution may be to add a Cube IDE example project instead of a IAR workbench one in the software example of the STEVAL-PTOOL2V1.
Best Regards,
Alexander
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.