Skip to main content
LAlva.2
Visitor II
November 16, 2022
Question

Fault pin on STMPS2161

  • November 16, 2022
  • 1 reply
  • 547 views

I was looking at a schematic that uses the STMPS2161 and the FAULT pin is pulled up to VIN (open drain), however it is not being read. Is it necessary to pull-up this pin if it will not be used or can it be left floating?

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    November 18, 2022

    Welcome, @LAlva.2​, to the community!

    The FAULT pin of the STMPS2161 is only used to signal an error. If you do not query it anyway and thus do without this signalling, you can simply leave it open and unconnected.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.