cancel
Showing results for 
Search instead for 
Did you mean: 

Stm mat target external mode demo example(nucleo f446ze) not working

MAziz.1
Associate II

Hello,

I am using stm 32 nucleo f446ZE LQFP 144, MATLAB 2020a, StmcubeMX 5.6.0, Keil V5.31.0.0. STM MAT TARGET rev 2.5. I am using stm32 demos>External mode> nucleo f446ze example(as I am also using stm32 Nucleo f446ze board). I followed the stm mat target pdf/handson script as well. So When I am Starting "build start and run" from SIMULINK, Build is succesful but after that I am having error"Launcher:startApplication(): error with getApplicationExecutable()" and the main.c file of Keil has showing missing "#include "F446ZE_external_mode.h". I tried so many things, (In settings I am using USART3 PD8 and PD9 pins as they are default for 144 pins MCU). But still I am unable to identify what is the cause of the error. Please help me in this regard. Just a thought - I am using keil V5.31.0.0 and in the pop of the simulink settings the version of keil is V5.27, Is this thing making an issue? I am using the correct COM Port, with correct baud rate of USART3.

0693W000004IaIXQA0.png0693W000004IaISQA0.png0693W000004IaINQA0.png0693W000004IaIIQA0.png0693W000004IaIDQA0.png0693W000004IaI3QAK.png0693W000004IaHyQAK.png

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Grege.1
Associate II

Hi,

I’m having the exact same problem, did you find any solution?

thanks.