Skip to main content
Associate
January 28, 2025
Question

wm-sg-sm-42: too much slow reading downlink messages on serial port

Hi,
There is someone that can help me with this issue ?
I updated the firmware correctly to the latest version: sm42_monolithix_v4.0.1.hex
I'm connecting via OTAA to TTN and it works fine.
For the first message I have a few seconds from uplink message and downlink message.
For the second message I have a few minutes (always 2 minutes and 12 seconds) from uplink message and downlink message.
Can I speed up the read of the downlink messages ?
 
Below there are the log of the serial command read:
 
Sending request: AT+JOIN=1 at 2025-01-27 15:47:39.911145
Received response: '# OK' at 2025-01-27 15:47:39.971146
Received response: '# +JoinAccepted' at 2025-01-27 15:47:48.325081
Transitioning from AT_JOIN to AT_SENDB1 at 2025-01-27 15:47:48.325166
 
Sending request: AT+SEND=2,50494E4731,1 at 2025-01-27 15:47:48.325312
Received response: 'OK' at 2025-01-27 15:47:48.365047
Transitioning from AT_SENDB1 to WAIT1 at 2025-01-27 15:47:48.365111
Sending request: AT+STAT at 2025-01-27 15:47:48.365143
Received response: '# +STAT=1,0,1,0,0,0,0,0,0' at 2025-01-27 15:47:48.373067
Received: 'OK' at 2025-01-27 15:47:48.373221
Received: '# +RCV=14,12,E79E39DFDE1FE76EDAE3DEFC' at 2025-01-27 15:47:55.941175

Transitioning from WAIT1 to AT_SENDB2 at 2025-01-27 15:47:55.941251
Sending request: AT+SEND=2,50494E4732,1 at 2025-01-27 15:47:55.941320
Received response: 'OK' at 2025-01-27 15:47:55.975199
Transitioning from AT_SENDB2 to WAIT2 at 2025-01-27 15:47:55.975306
Sending request: AT+STAT at 2025-01-27 15:47:55.975347
Received response: '# +STAT=2,0,2,0,0,217,8,1,1' at 2025-01-27 15:47:55.987187
Received: 'OK' at 2025-01-27 15:47:55.988255
Received: '# +RCV=14,12,E79E39DFDE1FE76EDAE3DEFD' at 2025-01-27 15:50:07.857554

Transitioning from WAIT2 to AT_SENDB3 at 2025-01-27 15:50:07.857626
Sending request: AT+SEND=2,50494E4733,1 at 2025-01-27 15:50:07.857685
Received response: 'OK' at 2025-01-27 15:50:07.891495
Transitioning from AT_SENDB3 to WAIT3 at 2025-01-27 15:50:07.891555
Sending request: AT+STAT at 2025-01-27 15:50:07.891583
Received response: '# +STAT=3,0,3,0,0,223,6,2,2' at 2025-01-27 15:50:07.903591
Received: 'OK' at 2025-01-27 15:50:07.904522
Received: '# +RCV=14,12,E79E39DFDE1FE76EDAE3DEDA' at 2025-01-27 15:52:20.075649

Transitioning from WAIT3 to AT_SENDB4 at 2025-01-27 15:52:20.075707
Sending request: AT+SEND=2,50494E4734,1 at 2025-01-27 15:52:20.075777
Received response: 'OK' at 2025-01-27 15:52:20.108809
Transitioning from AT_SENDB4 to WAIT4 at 2025-01-27 15:52:20.108959
Sending request: AT+STAT at 2025-01-27 15:52:20.109064
Received response: '# +STAT=4,0,4,0,0,217,7,3,3' at 2025-01-27 15:52:20.121105
Received: 'OK' at 2025-01-27 15:52:20.121622
Received: '# +RCV=14,12,E79E39DFDE1FE76EDAE3DDF4' at 2025-01-27 15:54:31.991944

Transitioning from WAIT4 to END at 2025-01-27 15:54:31.992002
State machine finished.
 
Thanks in advance for your support.
 
Marco
This topic has been closed for replies.

9 replies

Andrew Neil
Super User
January 28, 2025

That's the USI module on the old, obsolete I-Nucleo-LRWAN1, isn't it?

You'd have to go to USI for support with that - it's their module, and their firmware ...

 

Does the TTN console give any indication whether the delays are in TTN, or in the module?

Also, have you asked on TTN's forum?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
January 28, 2025

The board is board I-Nucleo-LRWAN2: https://www.st.com/en/evaluation-tools/p-nucleo-lrwan2.html

The delay is on the radio module, not on TTN.

 

Associate
January 28, 2025

I asked to USI to restore the github repository:

https://github.com/USIWPModule/USI_I-NUCLEO-LRWAN1