Skip to main content
Associate II
Sep 19, 2022 3:30 PM UTC
Question

Wifi Web Server

Hi All,

 I need to build a solution with a Web Server with Wifi interface.

I need to write html pages and so on, and drive an UART (implementing simple commands with a custom protocol).

What ST evaluation board do you suggest me?

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    Sep 19, 2022 5:14 PM UTC

    Aren't there some L4 and H7 based DISCO boards with WIFI modules?

    https://www.st.com/en/evaluation-tools/b-l475e-iot01a.html

    Could you do this with a current RPi ?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrei Chichak
    Lead
    Sep 19, 2022 11:31 PM UTC

    I did this with an STM32F407 with an ESP-8266 strapped to a UART. It was horrible. The 8266 AT command stack is/was an ill documented, brittle, piece and I had to write the whole HTML parser as well as the generator. You're not a "full stack web dev" until you've written the web server all of the way up to the css encrusted pages.

    Not recommended, 0 stars.

    On the other hand, once you get it going, you have a user interface on a headless embedded system and you don't have to write any client side applications as you would if you used bluetooth.

    I even started with ST's discontinued WiFi board. Oi was it premature. It would almost work, except for not being able to tell which page you were showing (handled by the WiFi processor) and it would just hand back an indication of which widget on the screen got hit, numerically, from the top of the screen, all screens handled the same way. So you couldn't tell the first widget of screen X from the first widget on screen BAR. Not useful. Sooooo much unbillable time spent on that mess.

    Nordic announced their WiFi offering recently. They did a really nice job on their bluetooth offerings, making it easier to get stuff going for the programming people. I haven't seen their chips show up on Digikey yet, but they tend to have nice dev boards with built on JLinks. Take a look.

    Either way, a web server wifi interface is a lot of work so far, and it's progressing, but very slowly.

    YMMV

    marco2Author
    Associate II
    Sep 20, 2022 7:16 AM UTC

    Thank you very much Andrei for your precious suggestions.

    I saw this project:

    https://github.com/khoih-prog/ESP8266_AT_WebServer#72-for-stm32-boards-to-use-serial1

    but it uses ESP8266 and now I have some doubts to use that solution.

    I saw also this:

    https://www.st.com/en/evaluation-tools/b-u585i-iot02a.html

    but the micro is too expensive.

    marco2Author
    Associate II
    Sep 20, 2022 7:17 AM UTC

    Thank you Tesla for your suggestion.

    I don't understand if there is firmware code with Web Server example inside.

    I have to check.

    marco2Author
    Associate II
    Sep 20, 2022 1:14 PM UTC

    Hi all,

    I found :

    https://os.mbed.com/teams/ST/code/DISCO_L475VG_IOT01-wifi_http_server/

    Based on INVETEK ISM43362-M3G-L44 module and mbed os.

    Ok, but the wifi module is very expensive.