Skip to main content
michael
Associate III
April 9, 2008
Question

trouble with ISR driven UART + loopback

  • April 9, 2008
  • 3 replies
  • 661 views
Posted on April 09, 2008 at 07:08

trouble with ISR driven UART + loopback

This topic has been closed for replies.

3 replies

kais
Associate
May 17, 2011
Posted on May 17, 2011 at 09:51

Hi,

could you please calrify more:

what do you mean by this?

''the ISR is invoked for the same character! ???''

Regards,

Eris.

michael
michaelAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:51

Hello all,

Here is the situation: I configure my UART to support loopback and to generate an interrupt when the fifo is 1/2 full but it goes wrong even if the fifos are disabled. the thing is that even I do acknowledge the interrupt, the ISR is invoked for the same character! Please note: this happens even if I send a single character!

This is the ISR:

Code:

<BR>unsigned char l_data = UART1->DR ; <BR> <BR> <BR> UART_ClearITPendingBit(UART1, UART_IT_Receive) ; <BR> //UART_ClearFlag(UART1) ; <BR> <BR> VIC0->VAR = 0; // Acknowledge Interrupt <BR> VIC1->VAR = 0; // Acknowledge Interrupt

UART1->DR keeps on containing the same character!

I know the UART works, because when I disable UART1_IMSC's RXIM bit, interrupts are not longer generated but the data ends up on the bus (still looped back though...).

Can you help me?

[ This message was edited by: michael.tamir on 09-04-2008 09:15 ]

michael
michaelAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:51

Hello and thanks for your reply,

I mean that every time the ISR is invoked, I read the same character from the DR register! The ISR is invoked continuousely, delivering the same character.