cancel
Showing results for 
Search instead for 
Did you mean: 

RF LTE-M evaluation on B-L462E-CELL1

Asmaa
Associate

Hello,

I'm working on LTE-M protocol and I would like to use B-L462E-CELL1 to evaluate the RF performances and characteristics of LTE-M protocol.
I would like to know, if it test tools/software to control the LTE-M chip in order to be the wanted mode is released or not?
I need this test software to program the RF device to transmit or receive mode, by defining the frenquecy and the transmit power... In order to test the following items:
- Tx Power / Frequency error
- Modulation accuracy
- Spectrum Mask
- Channel Testing
- Sensitivity

Could you please specify if this kind of control is possible and could be delivered for B-L462E-CELL1?
Thanks and Best Regards,
Asmaa

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Asmaa, to the community!

The LTE-M module in the B-L462E-CELL1 is from Murata, who you should contact for such special requests. However, such modules have also been discussed here in the community, e.g. here.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.