Skip to main content
Associate II
Mar 12, 2025 8:10 AM UTC
Solved

"No device found on target" trying to flash XM125 radar board with ST-Link V2.

I'm currently experimenting with an XM125 radar board . As seen on page 15 of the module's datasheet, this board essentially contains an STM32L4 MCU with the necessary external components and the radar sensor. All pins of the MCU are exposed through the board. So, essentially, I'm connecting directly to the STM32L4.

My Problem

I'm struggling with flashing something to the controller. I know this has been asked (and solved) a thousand times, but I simply cannot find the problem here.

When attempting to flash a default project by the manufacturer using an ST-Link V2 (genuine, not clone), I get the following output in STM32CubeIDE 1.17.0:

STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Target no device found

Error in initializing ST-LINK device.
Reason: No device found on target.

STM32CubeProgrammer (2.19.0) gives a very similar output:

12:52:16:265 : UR connection mode is defined with the HWrst reset mode
12:52:16:390 : ST-LINK SN : 37FF6F063143433923131843
12:52:16:391 : ST-LINK FW : V2J45S7
12:52:16:391 : Board : --
12:52:16:391 : Voltage : 3,23V
12:52:16:392 : Error: Unable to get core ID
12:52:16:392 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
12:52:16:404 : Disconnected

I've also tried pulling BOOT high during startup and changing the reset modes between Software, Hardware and Core, but the result was the same.

My Setup

I'm using a serial-to-usb interface stick to generate the source voltage of 3.3V. I'm additionally using a voltage divider to get the 3.3V down to 1.8V, since this voltage is required by the radar sensor. The following schematic outlines my setup:

schema.png

In the attachments, you find an image of my setup, and my test project.

This topic has been closed for replies.
blank_supportgisBest answer
Associate II
Mar 13, 2025 12:12 PM UTC

Yes, shortening the wires worked.  I'm gonna be honest, I was reluctant to clean up, because I didn't think it would help, but it did.

I've connected all dupont headers I soldered to the XM125 module directly to the ST-Link now, except for the power, which still comes from the breadboard (I need to get my 1.8V from somewhere). So, apparently, the problem was with the SWDIO and SWDCLK connections.

Anyway, thanks a lot to everybody for their help and patience!

21 replies

TDK
Mar 12, 2025 12:58 PM UTC

How much power is drawn on 1.8V? Might be being pulled too low.

Why are most of the grounds not connected?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Mar 12, 2025 1:12 PM UTC

The radar sensor isn't activated and therefore draws almost nothing, my multimeter isn't even sensitive enough. The overall current draw is around 13mA.

As for the unconnected grounds, I have no excuse but laziness. I figured, one ground connection should be good enough for testing. Am I wrong here?

TDK
Mar 12, 2025 1:23 PM UTC

For STM32 ground pins, they all need connected. I don't have information on how the module grounds connect to STM32 grounds. Probably that's worth checking out. A connectivity check between them might yield an answer.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Mar 12, 2025 1:06 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Mar 12, 2025 1:25 PM UTC

Yes, I tried acconeer's developer section But I didn't find any help there for my particular problem.

I think, this is a standard STM32 related question that isn't made special by the radar module. The XM125 is essentially a bare minimum STM32 MCU with one additional sensor. 

Andrew Neil
Super User
Mar 12, 2025 2:07 PM UTC

@blank_supportgis wrote:

I think, this is a standard STM32 related question that isn't made special by the radar module. 


But there could be something in their design that needs to be taken into account.

eg, have the locked-out the SWD access?

They have their own forum: https://support.acconeer.com/support/home

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 12, 2025 2:11 PM UTC

Have you tried connecting under hardware reset ?

Does  this ST-Link work with other targets?

 

PS:

Are you sure you have the ST-Link connections correct?

There was a case recently where the problem was misinterpreting the ST-Link pinout...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Mar 12, 2025 3:31 PM UTC

I tried connecting under hardware reset with the same result.

I currently don't have access to other targets, but I can check this tomorrow and let you know. I do have access to another ST-Link however. Same result.

I've checked the connections again using the XM125's datasheet and the ST-Link's datasheet and also verified proper connectivity with a multimeter. The wiring is as shown in my schematic.

blank_supportgisAuthorBest answer
Associate II
Mar 13, 2025 12:12 PM UTC

Yes, shortening the wires worked.  I'm gonna be honest, I was reluctant to clean up, because I didn't think it would help, but it did.

I've connected all dupont headers I soldered to the XM125 module directly to the ST-Link now, except for the power, which still comes from the breadboard (I need to get my 1.8V from somewhere). So, apparently, the problem was with the SWDIO and SWDCLK connections.

Anyway, thanks a lot to everybody for their help and patience!