Skip to main content
kobi_hayun
Associate III
March 10, 2005
Question

PC SPI Protocol

  • March 10, 2005
  • 2 replies
  • 712 views
Posted on March 10, 2005 at 12:42

PC SPI Protocol

This topic has been closed for replies.

2 replies

kobi_hayun
Associate III
March 10, 2005
Posted on March 10, 2005 at 11:39

Hi Everybody

Is anyone know of PC SPI protocol.

I need this in order to down load my final firmware (I dont have debug port in the final design).

Thanks

HKobi

fggnrc
Associate III
March 10, 2005
Posted on March 10, 2005 at 12:42

Perhaps I am wrong, but I am not aware of a PC SPI protocol.

SPI stands for Serial Periferal Interface.

The communication takes place between a master and a slave.

Both of them use a shift register that is updated by means of three wires: MISO (master in - slave out), MOSI (master out - slave in) and SCK (serial clock).

The data transmission is byte-oriented, but there is no protocol that states the meaning of the exchanged data.

To talk to a PC, it is better to use a microcontroller with a SCI (Serial Communication Interface). In this case you have to use a MAX232 to make the signal compatible with RS232 (aka COM ports of a PC).

It is more difficult to interconnect a PC with SPI, since you have to build custom hardware and attach it to a parallel port.

Even if you have a communication mean with the PC, it is up to you to implement the In Application Programming.

I suggest you to read the datasheet of the microcontroller that you are using, the ''Flash Programming Reference Manual'', AN1576 and AN1576.

Regards

EtaPhi