Skip to main content
Visitor II
February 10, 2025
Question

Parameter Definitions of L9678P

  • February 10, 2025
  • 1 reply
  • 695 views

Hi,

I'm using L9678P. I’d like to confirm the specific definitions of these parameters:

  • Is 1~10KΩ the detectable range?
  • Are the conditions in the "Condition" column strongly correlated with the parameter values?
  • What does "Equivalent to resistance range" mean in this context? 
  • Snipaste_2025-02-10_10-20-42.pngSnipaste_2025-02-10_10-21-12.png
This topic has been closed for replies.

1 reply

Andrew Neil
Super User
February 10, 2025

@Yang1 wrote:
  • Is 1~10KΩ the detectable range?

No - see the text description in the 'Conditions' column.

1-10k is the area of uncertainty between "guaranteed to be detected" and  "guaranteed to not be detected

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.