Skip to main content
shinnlin
Associate III
September 14, 2004
Question

Momory modification problem on RVDebug 1.6.1

  • September 14, 2004
  • 3 replies
  • 686 views
Posted on September 14, 2004 at 14:49

Momory modification problem on RVDebug 1.6.1

This topic has been closed for replies.

3 replies

shinnlin
shinnlinAuthor
Associate III
September 13, 2004
Posted on September 13, 2004 at 07:18

When I use RVDebug to debug our own target board, I always encounter a problem on modifying the Register values.

My steps are:

1. view the GPIO1 registers

C0: 0x7FFF

C1: 0x7FFF

C2: 0x0

D : 0x59FF

2. set C1 to 0x0

3. set C2 to 0x7FFF

after step 3, all C0, C1, C2 and D are showed 0x3838

The momory content at 0xE0004000 is

0x38 0x00 0x01 0x00 0x38 0x00 0x01 0x00

0x38 0x00 0x01 0x00 0x38 0x00 0x01 0x00

0x38 0x00 0x01 0x00 0x38 0x00 0x01 0x00

........

Anything goes wrong ?

Besides, sometimes the RVDebug doesn't let me modify the memory content....

shinnlin
shinnlinAuthor
Associate III
September 14, 2004
Posted on September 14, 2004 at 03:17

Do you refresh the Register window after all modifications ?

The C0 value seems not the same as displayed in Memory window.

[ This message was edited by: Shinn on 14-09-2004 06:52 ]
shinnlin
shinnlinAuthor
Associate III
September 14, 2004
Posted on September 14, 2004 at 03:18

I found that the crash problem is on our target board only,

and maybe the setting causes one short situation and crash the system.

Besides, I can't modify the 15th bit of all GPIO groups to 1 both on our target board or on STR710 Eval-Board.

The display on Register window and Memory window are not the same for bit It even has opposite value between two windows.

see attached JPEG for example.

Don't need specific operation sequence to reproduce this.

Do yo have this circumstance on your side ?

[ This message was edited by: Shinn on 14-09-2004 06:50 ]

________________

Attachments :

reg01.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtNf&d=%2Fa%2F0X0000000aP9%2FKkWewv8H8r1ZAuw7jCk9ZNbJWaagLyNE.VLZWsiv5nk&asPdf=false

reg02.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtMY&d=%2Fa%2F0X0000000aP3%2F.q0mt431cIxvXcye3xOLe_Imi0Y2w30tavEGt8WhVBM&asPdf=false