Skip to main content
sangeeta
Associate
May 17, 2008
Question

mapping RAM area for STR730

  • May 17, 2008
  • 2 replies
  • 791 views
Posted on May 17, 2008 at 09:50

mapping RAM area for STR730

This topic has been closed for replies.

2 replies

sangeeta
sangeetaAuthor
Associate
May 17, 2008
Posted on May 17, 2008 at 04:25

Hi,

I am using STR730 microcontroller, its RAM size is 16k, but I need more RAM space for my application.

How can I have more RAM space with the same processor?

Can I remap RAM or can i used space space from Flash for RAM?

Sang

kleshov
Associate
May 17, 2008
Posted on May 17, 2008 at 09:50

If you have 16K bytes of RAM, that's how much RAM you have, and no amount of remapping will change that fact.

I think you were going to ask a different question, which is

'Even with this limited amount of RAM, is it possible to make my application work, maybe utilizing Flash somehow?'

Well, only you can answer that question, since you provided no information about your application.

Regards,

- mike