cancel
Showing results for 
Search instead for 
Did you mean: 

L200CH and L200CV _ Power and Current Regulator

JSong.4
Associate

Can some one be so kind to let me know the difference between those 2 regulators?

Is it bending angel of the pin or the SPQ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @JSong.4​, to the community!

L200 has been discontinued for a long time, but the following assignment applied:

  • L200CH: Pentawatt package, horizontal mounting, i.e. component resting on PCB and parallel to it, 90° angled THT pins
  • L200CV: Pentawatt package, vertical mounting, i.e. component standing on PCB straight THT pins
  • L200T, L200CT: TO-3 package

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JSong.4​, to the community!

L200 has been discontinued for a long time, but the following assignment applied:

  • L200CH: Pentawatt package, horizontal mounting, i.e. component resting on PCB and parallel to it, 90° angled THT pins
  • L200CV: Pentawatt package, vertical mounting, i.e. component standing on PCB straight THT pins
  • L200T, L200CT: TO-3 package

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.