cancel
Showing results for 
Search instead for 
Did you mean: 

JTAG Reset

sjo
Associate II
Posted on January 16, 2006 at 06:35

JTAG Reset

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sjo
Associate II
Posted on January 12, 2006 at 05:45

Could ST confirm if the jtag cell is reset when RSTIN is asserted, this would explain what i am seeing.

Regards

sjo

sjo
Associate II
Posted on January 16, 2006 at 06:35

I am working on an open source project called OpenOCD -

http://developer.berlios.de/projects/openocd

This is a arm7/9 debugger/programmer gdb/telnet server.

One of the methods of halting the program from hardware reset is to set a breakpoint on 0x00 and reset device.

This works if the jtag cell is not reset under device reset.

For the str7 a software reset will have to be used instead - simliar to the lpc devices.

Regards

sjo