cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH st7c2334j4

chill_just_chill
Associate II
Posted on April 14, 2003 at 06:51

FLASH st7c2334j4

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
chill_just_chill
Associate II
Posted on April 10, 2003 at 15:10

Actually, I need to write a program that tests the FLASH of the st7c2334.

I need to program al the memory bytes to '0' and than check.

I need to program al the memory bytes to '1' and than check.

If the checks correspond, the flash is ok.

Has anyone got an idea how to do that ?

tia

Chr

sjo
Associate II
Posted on April 11, 2003 at 09:40

Because you are using a CFlash part you will need an external micro to put the device into programming mode (IAP is not available on this device) and just upload a custom bootrom.

You could adapt my prgrammmer to do this. (www.spen-soft.co.uk)

Or if ST would document the 'RAM Exec' function of Visual Programmer you might be able to do it from there, but you would still need a means of uploading the custom bootrom.

Regards

Spen
chill_just_chill
Associate II
Posted on April 11, 2003 at 16:01

indeed,

that's just what I'm doing:

downloading code into RAM of st7 via ISP through another st7.

It's my thesis.

sjo
Associate II
Posted on April 11, 2003 at 17:45

Why don't you just copy my programmer - www.spen-soft.co.uk

You could remove the flash and a few components and have a small pcb.

All the source and info is there

Regards

Spen
chill_just_chill
Associate II
Posted on April 11, 2003 at 23:48

I CAN program the flash of an st7, I have a much simpeler programmer than yours..

But I need a program that writes to flash from RAM

greetz

sjo
Associate II
Posted on April 14, 2003 at 06:51

If you can write to the flash then you must already have a bootrom which executes from RAM - I'm afraid I don't understand what you want.

Regards

SJO