Skip to main content
swiggers9
Associate III
September 29, 2006
Question

external interrupt on p1.11

  • September 29, 2006
  • 4 replies
  • 1019 views
Posted on September 29, 2006 at 06:52

external interrupt on p1.11

This topic has been closed for replies.

4 replies

swiggers9
swiggers9Author
Associate III
September 26, 2006
Posted on September 26, 2006 at 06:41

Hi,

I have an external adc which toggles a pin when conversion is ready. this pin is connected to p1.11 of a STR710FZ2.

I would like an interrupt to be generated when the pin toggles low but it doesn't seem to work.

Any suggestions why?!

here is my code

Code:

/***************************************************/

/* INIT ROUTINE

/***************************************************/

config_gpio_port(PORT_1, 0x0001 << EXAD_DREADY, GPIO_INPUT_PP );

XTI->MRH = 0x00;

XTI->MRL = 0x40;

XTI->TRH = 0x00;

XTI->TRL = 0x00;

config_irq_channel_priority(IRQ_CHANNEL_XTI, IRQ_PRIORITY_XTI);

EIC->IER |= 0x00000020;

XTI->CTRL = 0x00;

XTI->CTRL = 0x02;

/***************************************************/

void xti_isr(void) __arm

/***************************************************/

{

uint16 line_value;

line_value = XTI_InterruptLineValue();

XTI_PendingBitClear(line_value);

if(line_value == XTI_Line6)

{

external_adc_interrupt();

}

}

swiggers9
swiggers9Author
Associate III
September 29, 2006
Posted on September 29, 2006 at 04:54

is there nobody who knows what I'm doing wrong here?!

hichem2
Associate
September 29, 2006
Posted on September 29, 2006 at 06:46

Hello,

Could you tell me which tool-set and which board you use to develop your application?

Do you load you project in FLASH or RAM, What is the boot pin setting?

BOOTCR 16bit register allows you to know which memory is mapped to address 0, BOOTCR address is 0xA0000050

0xXXX0 -> FLASH

0xXXX2 -> RAM

0xXXX3 -> EMI bank0

regards,

Hich

swiggers9
swiggers9Author
Associate III
September 29, 2006
Posted on September 29, 2006 at 06:52

I'm using the MCBSTR7 evaluation board with a STR710FZ2 uC and uVision 3 from Keil as IDE.

I load the code into flash.

The pin BOOT_EN is connected to ground so boot0 and boot1 have no effect.

Do you need any more information?