cancel
Showing results for 
Search instead for 
Did you mean: 

button interrupt?

mpj
Associate II
Posted on August 10, 2006 at 07:03

button interrupt?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
mpj
Associate II
Posted on May 17, 2011 at 09:31

Hi,

Can someone point me to a button interrupt example for the STR910-EVAL board.

Thanks

Michael

anis
Associate II
Posted on May 17, 2011 at 09:31

Hi Michael,

There is an example of button interrupt in the WIU folder in the examples provided with the standard library.

Best regards,

STARM

Posted on May 17, 2011 at 09:31

hi,

I found the problem in WIU example

I need to detect a usb cable removal so I'm trying to use pin P75

as USB voltage detecting.

In the example I changed the output pin to P70 and

when I change the output state the WIU_PR bit related to this

pin is set.

The GPIO7OUT is configured as 0x0001

I'd like to know if this is a normal behavior.

mpj
Associate II
Posted on May 17, 2011 at 09:31

Thank you.

Michael

Posted on May 17, 2011 at 09:31

Hi,

I'm trying to use the WIU demo.

If I contine to press the button the IRQ is always asserted.

Could you let me know if is possible to assert the irq only

with a rising or falling edge?