cancel
Showing results for 
Search instead for 
Did you mean: 

uPSD3212 Memory Mapping Help

tong
Associate II
Posted on April 24, 2004 at 21:43

uPSD3212 Memory Mapping Help

2 REPLIES 2
tong
Associate II
Posted on May 17, 2011 at 12:00

Hi

I am using the uPSD3212, and planning to have the primary flash as program space and the secondary as the data space.

The primary flash is devided in to 4 sector of 16K and I am planning to stack them up from 0x0000 to 0xFFFF.

The socondary flash is 16K and I am planning to have it as two banks of 8K each and

Please tell me if this will work ok or not?

tong
Associate II
Posted on May 17, 2011 at 12:00

Thank You

Maybe I will ask you some more question when I do this.

Since you have done it. If you don't mind.

Thanks again.