Skip to main content
infoinfo994
Visitor II
December 7, 2011
Question

STR912: problem writing boot code to Bank0

  • December 7, 2011
  • 15 replies
  • 2847 views
Posted on December 07, 2011 at 22:48

Okay, I've learned how to move code to Bank1, and it executes properly.

After having some problems getting bank1 booting to work, we decided to instead try copying our firmware into an external Flash chip and validate it, then switch to code which is entirely in Bank1, to write from the external flash back into bank0.

I first wrote and tested code to enable unused sectors in Bank1 and write/verify code; this works fine.

Now I'm trying to write code from Ext Flash to bank0:

//**************************************************************************************************

u8 *src = (u8 *) ALT_FEPROM ;

u8 *dest = (u8 *) (0) ; // Bank0 Sector 0

bytes_remaining = datum[0] ;

unsigned flags = disable_IRQ(); // make sure nothing tries to execute from bank0 !!

set_led_green_on() ;

while (LOOP_FOREVER) {

wlen = (bytes_remaining > SIZE_64K) ? SIZE_64K : bytes_remaining ;

// this function is executing successfully...

if (feprom_program_enable_bank0(dest, BANK0_FM) == FALSE) {

break;

}

set_led_red_on() ;

delay_250msec(4) ;

u32 u32SectorAddr;

// if the physical address does not belong to any of the internal flash sectors, fail.

if (!bank0_bGetBankSecAddrByPhyAddr((uint) dest, &u32SectorAddr, NULL)) {

break;

}

// 12/07/11 - here is the show-stopper...

// If I call this function, which writes to two registers in the internal flash-programming interface,

// the sector erase proceeds successfully, but the code never returns to here...

bank0_EraseSector(u32SectorAddr); // Erase the sector

//**************************************************************************************************

However, as the comments reflect, the sector-erase function never returns.

I used OpenOCD via the JTAG interface, to look at bank0 space after the crash, and it appears that the erase *did* occur, but the function never returns.

bank0_EraseSector() contains only two writes to the STR9 CUI interface:

//**************************************************************************************************

static void bank0_EraseSector(vu32 FMI_Sector)

{

/* Write an erase set-up command to the sector */

*(vu16 *)FMI_Sector = 0x20;

/* Write an erase confirm command to the sector */

*(vu16 *)FMI_Sector = 0xD0;

}

//**************************************************************************************************

So why does this crash? What else do I need to do to make this work?

I tried remapping bank1 to boot bank and bank0 to non-boot bank, using

// FMI_BankRemapConfig(0, 6, 0x80000, 0) ; // this crashes the board immediately!!

but that doesn't work either...

Our system: STR912 512K/32K
This topic has been closed for replies.

15 replies

v_tamakov
Associate
December 27, 2011
Posted on December 27, 2011 at 17:08

Dear Sir, I have one problem with MCU STR912FA46; when code of program less then 512 kB, MCU is working well. But when code of program more then 512 kB, my program no working and MCU going on the PDAbort vector. Because program is good and I add only BMP-file for presentation. I am using Keil MDK 4.00. All setup for FMI is correct. Where are I can mistake? Best regards. Vladimir,

gupta2
Associate
May 7, 2012
Posted on May 07, 2012 at 12:21

Hi...

I am also experiencing similar kind of problem as mentioned above.  I am working on str912faw44, putting bootloader into bank1, through bootloader code i am programming bank 0 and running it after remapping. My problem is if bank0 code size is less than 8k, everything works fine, but if code size becomes more than 8k it doesn't get downloaded properly into bank0.

Pantuca.Erwin
Visitor II
May 12, 2012
Posted on May 12, 2012 at 05:50

a data abort usually indicates an invalid address.  you might check the assembler code just before the abort for any such invalid address access.

gupta2
Associate
May 16, 2012
Posted on May 16, 2012 at 08:32

Hi..

just want to be more specific for my problem. Through bootloader code I am writing main app code in FMI B0S0 starting from the memory location 0x80000 onwards. If code size is <0x2000 bytes no problem, but if size is greater than 0x2000 bytes(>8K) and when i try to write at 0x82000, something goes wrong. On debugging i got that when try to write to this location FMI_FLAG_PS (program failure) become set, because corresponding FMI_FLAG_SPS (sector protection) is also set, but sector write protection is disabled before start writing, thats why it could become possible to write upto 0x81fff.  I couldn't understand whats happening, can that location corresponds to OTP, or something wrong with remapping. Please suggest.

Pantuca.Erwin
Visitor II
May 17, 2012
Posted on May 17, 2012 at 15:17

have you reviewed the errata sheet?

gupta2
Associate
May 19, 2012
Posted on May 19, 2012 at 11:44

yea..i had gone through the errata sheet as well and tried for workaround for TCM order bit through assembly language, but still no help. Other conditions mentioned in sheet were not in accordance with my problem. Any other idea???

Pantuca.Erwin
Visitor II
May 21, 2012
Posted on May 21, 2012 at 08:26

try to write at 0x82000 first?

gupta2
Associate
June 5, 2012
Posted on June 05, 2012 at 09:16

Pantuca.Erwin
Visitor II
June 6, 2012
Posted on June 06, 2012 at 10:07

just a clarification, in your original problem, it was related to size?  so now it is really not a size issue, just that you cannot write 0x82000?

gupta2
Associate
June 18, 2012
Posted on June 18, 2012 at 10:43

Hi..

just wanna to draw attention to one more thing. On this forum only in some earlier conversations i have read exactly the same problem as mine, they also couldn't write beyond 8192 bytes in secondry flash. Rest all other things were almost same as i am using. They have mentioned that this is related to CSx bit mapping and suggested to correct it, by setting this they were claiming that there program was working.

I also tried for setting the CSx bit through STR91x_CFG.s and again tried for downloading the code, but i again got stuck at 0x82000 :(

If you have any idea w.r.t CSx bit please help me. Is it related to this only or there is any other thing also that i am overlooking.

Bye. Good day.