2023-09-22 02:29 AM
Hi Team,
I would like to know the Part #STPS24045 is qualified AEC. If not, can you help me to get the Diode with a higher current rating (min: 220A of forward current) and AEC qualified. Thanks, in advance.
-
Gopi
2023-09-22 05:33 AM
Welcome @Gopi-N, to the community!
The STPS24045 has no AEC qualification, so it is not automotive approved.
However, there is a possible suitable Schottky diode with min 220A in the portfolio of STMicroelectronics: the STPS240H100TV1Y, which could just about suffice with 100V and 2x120A, is AEC-Q101 qualified and available with PPAP.
Hope it helps?
Good luck!
/Peter