2004-09-28 01:38 AM
2004-09-27 07:58 PM
Dear sir,
while I use St7MDT10-EMU3, there is an error messag like this. ** Connection error (usb://usb): gdi-error in hds:[10004] no Communication with emulated mcu Could anyone tell me how to solve this problem. Best Regards, Mucinterest2004-09-28 01:38 AM
There seems to be a connection error, so you can verify the following:
1. If you are using STVD7 3.0, In the Debug Instument Tab, select the Port at which you have connected the emulator. If you are using old version of STVD7, in the emulator settings select the Port correctly. 2. Try changing the Microconnect (If you have an Extra?) 3. Check the Flex-Cable that you are using