2004-12-06 03:06 AM
SPI's TEISF flag doesn't reset when user reads SPISTAT register
2011-05-17 03:04 AM
First, the bit definitions of SPI status is displaced with the corresponding bits in Table 63, page 116/230, the Sept. 2004 version of uPSD33xx data manual.
I worked on the SPI interface on the DK3300 recently, and I found that SPI's TEISF flag doesn't reset when user reads SPISTAT register. Is there anybody else finding the same symptom? I don't think this is a big issue, but I just make sure my uPSD is working correctly.