Skip to main content
kebap
Associate II
May 11, 2005
Question

How to run a program?

  • May 11, 2005
  • 3 replies
  • 905 views
Posted on May 11, 2005 at 04:31

How to run a program?

This topic has been closed for replies.

3 replies

rk1
Associate
May 17, 2011
Posted on May 17, 2011 at 12:06

hi,

no, there is no ''start condition''. but make sure to configure/trigger or disable the watchdog.

if you want to know if the microcontroller is running, configure 1 pin as output and toggle it in an endless loop, and then look at the pin (i.e. with an oscilloscope).

kebap
kebapAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:06

Hello!

We have a problem with our uPSD3254a.

We have load a demo-program(initialize a display and put out a character)

with PSDsoft Express to our microcontroller,but the LCD doesn't display anything.

Does a start condition for the microcontroller exist?

What have we to do, to run the microcontroller.

Regards preines

thomasthanner9
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:06

Hello,

there are actually two conditions that can stop a uPSD from running. First is the Watchdog as already mentioned by rk__. Second is the pullup at the USB_D- pin. This pullup is required even on non USB-devices. Maybe that is what is missing from your design?