cancel
Showing results for 
Search instead for 
Did you mean: 

EMIF08-LCD04M16 PIN OUT?

JSten.3
Associate

I am looking to get confirmation on the pin out of EMIF08-LCD04M16 in QFN package. The datasheet makes no mention of this. I assume that it is a pass through type, where pins opposite each other are connected through the filters, and that the exposed pad is ground. Can someone confirm this, or correct my assumption?

Thanks

Joel

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @JSten.3​, to the community!

Sorry for the inconvenience - your assumption is correct: it is a pass thru device, where the opposite pins are input/output and the exposed pad is GND.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JSten.3​, to the community!

Sorry for the inconvenience - your assumption is correct: it is a pass thru device, where the opposite pins are input/output and the exposed pad is GND.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.