Skip to main content
FBert.3
Visitor II
April 6, 2022
Solved

how to change motor and power board configuration values and topology in MCSDK 6.0?

We are developing using STEVAL-CTM009V1 with two insulated in phase shunt.

We are not able to find how to text edit json data to configure custom board.

Could you please suggest how to go on?

Thanks

This topic has been closed for replies.
Zied b.Best answer
ST Employee
August 24, 2023

hello @Jedijump ,
The STEVAL-CTM009V1 Power board will be supported in the next version of the MCSDK which is version 6.2.0. This version will soon be available for download.
Regards

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."

5 replies

cedric H
ST Technical Moderator
April 6, 2022

Hi @FBert.3​,

The MCSDK 6.0 introduces a brand new way to describe boards.

Our goal is that users will have the same comfort with their own boards than with ST boards.

For the moment, you can add your own boards in the asset folder located in your installation directory of the MC_SDK:

C:\Program Files (x86)\STMicroelectronics\MC_SDK_6.0.0\Utilities\PC_Software\STMCWB\assets\hardware\board\[power|inverter|control] and they will be proposed at the next run of the Workbench.

As it is not very convenient for now, we plan to add very soon an easy way to import json description from the WB UI.

Regarding the description of the board itself, we are about to release a complete documentation on the wiki page. I will update this post as soon as the documentation is available.

The MCSDK-6.0 should be consider as a preview with only few G0 and G4 boards supported, and few power boards. We are working hard to bring back all the boards supported in 5.Y release in the next MCSDK-6.

Regards

Cedric

Associate
August 19, 2023

Hi Cedric,
Any update regarding how can we add our own power board in the Workbench? In MCSDK-6.0?
I would like to use STM's ctm009v1, but it is not listed as a power board inside the ST Workbench.

Look forward to your answer and solution.

Thank you.

Regards,

Jedijump 

Zied b.Best answer
ST Employee
August 24, 2023

hello @Jedijump ,
The STEVAL-CTM009V1 Power board will be supported in the next version of the MCSDK which is version 6.2.0. This version will soon be available for download.
Regards

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."
Associate
August 28, 2023

Hi Zied,

 

Thank you for your response. I will look forward to v6.2.0.

However, in the meantime if you can advise on how to specify two insulated in phase shunt in using STEVAL-CTM009V1, it will be good.

 

Sorry, I am not able to find the "Accept as solution" button, but I appreciate your solution.

Thank you.

Regards,

Jedijump

Associate
August 31, 2023

Hi Maxharry,

I am aware of the JSON requirement, but is there a document that I can refer to?

The STEVAL-CTM009V1 board uses 2 isolated current sensor (ICS), instead of the usual 3 shunt resistors. I do not know how to configure that in the JSON file. Other parameters can be done with reference to known power boards.

Appreciate if anyone can advise, because the MCSDK v6.2.0 has not come and I need to progress.

Thank you.