Skip to main content
RatheeshT
Associate III
February 17, 2021
Solved

Is there any interconnection / relation between port F12 and F13 on SPC560P Disp?

  • February 17, 2021
  • 5 replies
  • 1833 views

Hi Technical team.

I want to configure both F12 and F13 as input pin.

When i am trying to configure F12 and F13 as input pin in PinMap Editor , it gives error (attached the error screen).

I tried this on sample project "SPC560Pxx_RLA SERIAL Test Application for Discovery".

Hardware used : SPC560P Disp

Please suggest me your ideas to solve this issue

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello Ratheesh ,

    Cf reference manual,

    It is not possible to configure F12 and F13 with the same function (Ex: GPIO92).

    Best regards

    Erwan

    5 replies

    Erwan YVIN
    ST Technical Moderator
    February 17, 2021

    Yes ,

    You have tried to configure F[12] and F[13] to the same GPIO

    cf Screenshot and reference manual

    Best Regards

    Erwan

    0693W000008GQwAQAW.png

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    RatheeshT
    RatheeshTAuthor
    Associate III
    February 18, 2021

    Thanks for your immediate response

    From above conversation, My understanding is below,

    Port F12 and F13 are not available to configure/use as GPIO pin at the same time in the application

    We can use/configure either F12 or F13 only as GPIO at the same time .

    is my understanding correct?

    or

    If my understanding is not correct, Please provide the procedure to configure both F12 and F13 pins as GPIO in SPC5Stusio.

    Thanks in advance

    RatheeshT
    RatheeshTAuthor
    Associate III
    February 19, 2021

    Hello Erwan,

    Could you please provide your opinion on this.

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    February 19, 2021

    Hello Ratheesh ,

    Cf reference manual,

    It is not possible to configure F12 and F13 with the same function (Ex: GPIO92).

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    RatheeshT
    RatheeshTAuthor
    Associate III
    February 19, 2021

    Hello Erwan,

    Thanks for your support, I am closing this ticket. It is best