Skip to main content
FCola.1
Associate II
May 8, 2023
Solved

Bootloader not working with new SPC5Studio

  • May 8, 2023
  • 1 reply
  • 1272 views

Hi,

I have troubles with the new version of SPC5Studio.

I have made a bootloader with SPC5Studio V. 5.8.1 which is working fine but when I have remade it with the new SPC5Studio software it doesn't jump to application code.

 

This is what happens:

 

The bootloader starts correctly when I send the id upgrade message from CAN. It saves correctly the application code in Flash memory. After that, I turn off the device and then ,after few seconds, I turn on it. After few checks it jumps to the application code but here is when I saw two different behaviours : bootloader's code with SPC5Studio version 5.8.1 can jump to application code, the one with SPC5Studio version 6.0.0 fails. They have the same source code, same memory map and the only few changes are that which are generated with "Generate SPC5 Application" button. Any suggests? Could I receive SPC5Studio v. 5.8.1 version in order to compare the auto-generated code? Thanks in advance.

 

P.S.

 

Micro is SPC582B60E1

 

 

 

 

 

 

This topic has been closed for replies.
Best answer by Erwan YVIN

Hello Filippo ,

Sorry for the late answer

There is no difference between SPC5Studio 5.8.1 (32 Bits) and SPC5Studio 6.0 (64 Bits) in term of Low Level drivers.

have you got the same version of low level drivers (RLA) ?

    Best Regards

                  Erwan

 

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
August 28, 2023

Hello Filippo ,

Sorry for the late answer

There is no difference between SPC5Studio 5.8.1 (32 Bits) and SPC5Studio 6.0 (64 Bits) in term of Low Level drivers.

have you got the same version of low level drivers (RLA) ?

    Best Regards

                  Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.