Skip to main content
tjian.3
Visitor II
May 22, 2023
Solved

程�?Debug�?行时,�?行到此处,就�?�止了,这是为什么?

  • May 22, 2023
  • 2 replies
  • 1161 views

..

This topic has been closed for replies.
Best answer by Erwan YVIN

it seems to be a coredump issue.

Please check PC, R14 and R13

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
May 22, 2023

it seems to be a coredump issue.

Please check PC, R14 and R13

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Giuseppe DI-GIORE
ST Employee
May 22, 2023

In addition to Erwan's suggestion check also MCSR register and if MAV field (bit-19) is set then register MCAR contains the address of the fault.

Regards.