cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12TR PLEASE CONFIRM WHY THERE IS NO BODY MARK OVER THIS MOTION SENSOR IC.

USING.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @USING.1​ ,

there should be a indeed a marking on the top surface of the device package, like the one here below:

0693W000007ZJFDQA4.jpgCan you please send a picture of your device? Maybe it was discolored after soldering or application of a chemical coating...

-Eleon

View solution in original post

5 REPLIES 5
Eleon BORLINI
ST Employee

Hi @USING.1​ ,

there should be a indeed a marking on the top surface of the device package, like the one here below:

0693W000007ZJFDQA4.jpgCan you please send a picture of your device? Maybe it was discolored after soldering or application of a chemical coating...

-Eleon

Thanks for reply. But this is not mentioned anywhere in datasheet. Please clarify ?

Hi @USING.1​ ,

no, it is not specified in the datasheet...

This because the datasheet is generic, while the 2D matrix is related to the specific assy lot for the case tracking (it contains the product code, the week/year (usually in the format Y/WW) of assy etc...).

-Eleon

Thanks Mr Borlini for your prompt replies.

You're welcome @USING.1​ , hope this could be of some help for you.

-Eleon