Skip to main content
MHelk.1
Visitor II
January 16, 2020
Question

About MP23ABS1, Its Output voltage & frequency? Whether its output voltage will be superimposed or original waveform?

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    January 17, 2020

    Hi @MHelk.1​ , the output of the analog mic MP23ABS1 is basically ratio-metric. This means that if you supply the device with Vdd = 2.7V (the typical datasheet value), you will get an output offset of almost Vdd/2 (DC level value), with the signal superimposed on it. For example, if the input signal is a sinewave at 1kHz, 120dBSPL, being the sensitivity typ value -38dBV, the output signal will be DC level + sinevave at 1kHz of about 300mV peak. The output frequency is the same one of the acoustical input wave. Regards