Skip to main content
HIMAM.1
Associate
January 26, 2021
Solved

About FIFO of gyro sensor I3G4250D

  • January 26, 2021
  • 2 replies
  • 1032 views

Is it stored in the FIFO when the threshold of the INT1_THS register is exceeded?

Or is it stored regardless of the threshold of the INT1_THS register?

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @HIMAM.1​ ,

    if you intend the mechanical threshold of an external event, there is no trace of the interrupt in the FIFO (the INT1_THS is a configurable mechanical threshold).

    If you intend the programmable watermark level event (i.e. when the desired FIFO filling level configurable in the FIFO_SRC_REG (2Fh) register is reached), it can be enabled to generate dedicated interrupts on the INT2 (I2_WTM bit of CTRL_REG3 (22h)), as described in the datasheet p.17.

    I suggest you also to check the example available on Github for the i3g4250d_fifo_read.c.

    -Eleon

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    January 27, 2021

    Hi @HIMAM.1​ ,

    if you intend the mechanical threshold of an external event, there is no trace of the interrupt in the FIFO (the INT1_THS is a configurable mechanical threshold).

    If you intend the programmable watermark level event (i.e. when the desired FIFO filling level configurable in the FIFO_SRC_REG (2Fh) register is reached), it can be enabled to generate dedicated interrupts on the INT2 (I2_WTM bit of CTRL_REG3 (22h)), as described in the datasheet p.17.

    I suggest you also to check the example available on Github for the i3g4250d_fifo_read.c.

    -Eleon

    HIMAM.1
    HIMAM.1Author
    Associate
    January 28, 2021

    ​

    thank you for your answer.

    I got a better understanding with your answer.

    I will also check the example.