cancel
Showing results for 
Search instead for 
Did you mean: 

Which firmware should I use for a SPBTLE-1S?

MatteoFeatureJam
Associate II

I'm using the SPBTLE-1S BlueNRG-1 module on a custom PCB with a STM32L4R9ZI MCU. The SPBTLE-1S module and the main MCU are connected trough SPI. The SPBTLE-1S module can be flashed with various firmwares provided by ST. Which one should i choose? I would like to have it compatible with the code generated by the X-CUBE-BLE1 pack on CubeMX.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0