Skip to main content
Mhroczny
Visitor II
November 26, 2019
Question

STSW-BNRG-S2LP can't detect STEVAL-FKI001V1 devkit board

  • November 26, 2019
  • 0 replies
  • 487 views

Hello,

I have some problem with my STEVAL-FKI001V1 devkit board. When board is connected by USB to computer is visable as STMicroelectronics Virtual COM Port in device menager in Ports (COM and LPT) and as STM BlueNRG Family USB Device in Disk station. I register the board in Sigfox backend using SIGFOX_CLI_DEMO_FKI001V1 program from STSW-S2LP-SFX-DK. I can use USB - UART connection to send commands. The problem is in using STSW-BNRG-S2LP software package. When I chose right demo and right board it is always Board not selected or unplugged. Replugging board do nothing, the J7 and J6 jumpers are connected as USB mode. I tried reinstall drivers from STSW-BNRG-S2LP package, instalation was succeed and board is still visable as I describe above. Im using Windows 10. Thank you for any advices!

This topic has been closed for replies.