cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IDB008V1M MacOS

AOdonde
Associate

Hi everyone,
I recently got the STEVAL-IDB008V1M dev board, I am using a M1 Macbook Air. I tried to get Wise-Studio working but the application installs but does not open for me (yes I do have GNU make, and JRE installed).
So I decided to then install STM32CubeIDE and STM32CubeMX (WITH the X-Cube-BLE2, but I cannot seem to find any of the example code that comes with it). The aim was to hopefully use that to compile and flash my STEVAL-IDB008V1M. (This is a double sanity check that i have JRE installed and working properly I believe).
The question I have is, outside Wise-Studio (if it wants to work), is there a way to program and flash the STEVAL-IDB008V1M on a MacOS? Or is the answer use windows instead?


Thanks a bunch :)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0