cancel
Showing results for 
Search instead for 
Did you mean: 

SPFW04 File creation

Dmytro Medvid
Associate II
Posted on November 30, 2017 at 09:37

Hello everybody!

Is there a possibility in SPFW04 to POST and GET via HTTP not only from RAM, but from external SD card? 

Another question is whe i can`t create file bigger than 15360 bytes on external SD card? 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Gerardo GALLUCCI
ST Employee
Posted on November 30, 2017 at 10:26

Webserver (HTTP server) receive a request, then loops to find the file among all volumes. Example: 'GET index.html ' will result into searching for index.html into as 0:index.html, then 1:index.html, then 2:index.html, and 3:index.html. So, volume #0 (SD-Card/SPI Flash) has an higher priority than volume #3 (APP_Disk).

AT-Commands (HTTP client) accept the full path, including ':' to specify the volume number.

15KB is the size associated to RAM_Disk only (FW1.0.0); since FW1.1.0 you can decide this size too.

Posted on November 30, 2017 at 10:57

So, in FW1.0.0 i can`t create file bigger than 15Kb on SD card?

Posted on November 30, 2017 at 13:45

On SD-Card you can do what you want. No limits in size.