cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP register MC_STATE0 = 0xE8. Unknow state

VAlar.1
Associate II

I read 0xE8 at the MC_STATE0 register from the S2-LP.

The associated state 0x74 (0xE8>>1), doesn't match with any of the possible states:

typedef enum {

 MC_STATE_READY       =0x00, /*!< READY */

 MC_STATE_SLEEP_NOFIFO   =0x01, /*!< SLEEP NO FIFO RETENTION */

 MC_STATE_STANDBY      =0x02, /*!< STANDBY */

 MC_STATE_SLEEP       =0x03, /*!< SLEEP */

 MC_STATE_LOCKON      =0x0C, /*!< LOCKON */

 MC_STATE_RX        =0x30, /*!< RX */

 MC_STATE_LOCK_ST      =0x14, /*!< LOCK_ST */

 MC_STATE_TX        =0x5C, /*!< TX */

 MC_STATE_SYNTH_SETUP    =0x50  /*!< SYNTH_SETUP */

} S2LPState;

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0