Skip to main content
path321
Associate II
December 15, 2021
Solved

Query about BlueNRG-2N and BlueNRG-LP

  • December 15, 2021
  • 3 replies
  • 1305 views

Hello everyone,

I am developing a custom board with STM32L4 , and looking to include a "ready-to-use" BLE module, such as BlueNRG-2 series. I have in my possession X-NUCLEO-BNRG2A1 and tested it thoroughly.

In a previous question ( https://community.st.com/s/question/0D53W00001DNzSVSA1/preloaded-firmware-of-bluenrgm2sp ) found out that BlueNRG-M2SP comes "empty" and need flashing with specific firmware before actual use. After searching, I ended up between BlueNRG-2N and BlueNRG-LP processors.

Could you confirm that BlueNRG-2N doesnt need external flashing with firmware (or at least isnt necessary) and can work out of the box ? Is that also the case with BlueNRG-LP ?

This topic has been closed for replies.
Best answer by Sebastien DENOUAL

Hi @path321​ ,

Your statement is correct. BlueNRG-2N is already preflashed with DTM image and is so "ready to use". BlueNRG-2N is a chipset (not a module as per blueNRG-M2SP)

BlueNRG-LP is also chipset (BLE SoC) delivered empty.

Regards,

Sebastien.

3 replies

Sebastien DENOUAL
ST Employee
December 15, 2021

Hi @path321​ ,

Your statement is correct. BlueNRG-2N is already preflashed with DTM image and is so "ready to use". BlueNRG-2N is a chipset (not a module as per blueNRG-M2SP)

BlueNRG-LP is also chipset (BLE SoC) delivered empty.

Regards,

Sebastien.

path321
path321Author
Associate II
December 15, 2021

Thank you for the support Sebastien.

An additional question, Is ti correct to use the BOM of STEVAL-IDB008V2 as a compass for BlueNRG-2N application circuit described in its datasheet ? Are there any fundamental diffferences between the complimentary parts needed for BlueNRG-2 and BlueNRG-2N chipsets ?

Sebastien DENOUAL
ST Employee
December 15, 2021

Hi @path321​ ,

Yes : you are right.

In terms of chipset, BlueNRG-2N is a subset of BlueNRG-2 (some peripherals are not available on BlueNRG-2N). Now, packages are similar, BlueNRG-2 and BlueNRG-2N are pin2 pin compatible.

So, you can use BOM and layout from STEVAL-IDB008V2 - you can also optimize BOM by removing the low speed xTal (32Khz). Default BlueNRg-2N config is using internal low speed oscillator.

As said, BlueNRG-2N is preflashed and can work only in network processor mode (DTM) - not possible to reflash other image than ST ones.

Regards,

Sebastien.